Hi, having some issues with the DRV8412 driver. I've read descriptions of similar-sounding issues, but nothing that exactly describes this situation.
Setup:
-using a single +12V power supply for both main and boost voltage
-OC-adjust resistor is 22k
-driver used in dual full-bridge configuration to drive 2 linear actuators
-100% duty cycle
Symptoms:
-first board assembled worked without issues before sending to customer, but during testing, customer found that ~FAULT is asserted low and drivers are heating up
-second board assembled worked the first time it was tested (driving Actuator 1 outwards). Then, board failed in the same way as the first one: drivers no longer responsive, ~FAULT asserted low, drivers warming up without any load attached (even when input command is low/off).
Can anyone suggest follow-up diagnostic checks? I've measured the obvious things (supply power for driver chip, input commands) and nothing looks strange. The fact that everything worked at first makes me think it's not a basic routing or layout error.
From reading the datasheet, it sounds like this might be related to the duty cycle. I'm using 100nF bootstrap capacitors and there is a 47uF+1uF pair next to the power supply pins. The fact that everything worked initially though, makes me think the 100% duty cycle might not be an issue.
Alternatively, if someone can suggest a better chip for driving at 100% duty cycle, maybe I wouldn't have to worry about the PWM issue. Requirements:
-need to drive 3 linear actuators (https://www.firgelliauto.com/products/light-duty-rod-actuator, 1 at a time, at 5A max (more like 1A on average)
-drive voltage 9-14V