Hi, I have two brushed dc motors in series and the following link lists all the specifications. I will be running two 19.1V motors at 24V max
www.pittman-motors.com/.../14206-Brush-DC-Motor.aspx
I was hoping that this H bridge below would be able to help me
I'm hoping to hook both of the motors (in series) in the parallel configuration shown in the data sheet but I'd like to know if that configuration will be able to handle the amperage that the motors will demand and if you could provide me with a data sheet solely for the parallel configuration that'd be helpful.
Also maybe theres a better driver to handle the 6A (say cascading two different H bridges maybe?) that the motor would require for continuous torque seeing as how I need just a driver to handle 24V I'd appreciate any feedback or ideas that could help in controlling the speed and rotation of the motor