A new DRV8308DVM board and the Telco motor were wired as instructed in the Quick start User Guide SLVUA41D. The USB drivers and GUI composer were downloaded and installed per 5 steps of User Guide, section 2.1. However, when I run the launch.exe app it stops just seconds after displaying the main screen with red x's on all buttons and Initializing still in progress button, even after waiting 5-10 min and/or restarting the GUI several times. I tried reloading the software to no avail. Something is not initializing correctly in the GUI software. Green LEDs on the board show it's getting USB power and 24v for the motor. What am I doing wrong? There is only one COM port in use (COM5) during these attempts. Platform is Win7 on a desktop. Lots of memory, etc.