This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8432DKDEVM board input pwm issue

Other Parts Discussed in Thread: TMS320F28335

Hi,

I am using DRV8432DKDEVM evaluation board with parallel mode (i.e. MODE 3 M3 - 0, M2-1, M1-0)and have interfaced (GND, PWM 01, PWM 02) TMS320F28335 development board  for providing PWM pulses.

The issue i am facing is whenever i switch on  the PVDD signal (i.e 15Volt or 48 volt) input PWM signal gets distorted. and same when i off the PVDD supply it comes back.

NO error ( over current , over temp etc ) is occurred during this period. the signals at FAULT and OTW are constantly HIGH state.

Hardware wise i have connected the PWM signal from controller to board using wires.

Let me know if we can connect an external controller to generate PWM signal to this board?

Regards,

Nandakumar