Hi Team,
My customer would like to use internal RAM of DRV2604L.
I understood I can write RAM_DATA[7:0] at the RAM address(RAM_ADDR_UB:RAM_ADDR_LB).
Then, I have 2 questions.
I believe the selectable value of the RAM address(RAM_ADDR_UB:RAM_ADDR_LB) is 0~2047(0x000 to 0x7FF).
Is my understanding correct?
(2)
The datasheet shows "A waveform identifier is an integer value referring to the index position of a waveform in the RAM library".
Is "waveform identifier" and "RAM address" same meaning?
I believe it but also found "The waveform identifier range is 1 to 127" in datasheet, so I am confused.
Best Regards,
Yaita / Japan disty