Hi,
We have spent two days with an issue regarding this motor driver. We have constructed our own 2 layers pcbs and interface to the drv8308 using a mcu. Everything works perfectly. We can write to the registers and read them back and so on. No issues at all. The problem occurs when we raise the enable pin or use the register with the enpol set high. The drv8308 draws almost an amp of power and gets very hot, until enable is set low again. During this time the drv8308 continues to receive commands without any issues. We have this issue no matter if the motor is connected or not. We have two pcbs and it is the same on both of them. We have followed the schematics from the drv8308evm almost completely, allthough we use higher power mosfets. Same hall-sensors same components in the circuit. We have checked all connections several times and they show no problems what so ever. This seems weird. Anyone have any idea of what can be going on? Is this maybe a faulty batch of drv8308? Where is the power going?
Best regards,
Mikael Sundberg