This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Current control possible solenoid driver like a DRV110

Other Parts Discussed in Thread: DRV110

Hi,

 

I'm looking for a driver IC capable of current controllable solenoid drive like DRV110 in Automotive grade.

Not the PWM drive, I want to control the current in the IC.

Required functionality, overcurrent, overvoltage and o ver temperature protection and diagnostic functions.

The ablolute maximum voltage is 35V is required.

DRV110 we think is that it best, but since Q1 is the content, please tell me whether there is a device similar.

 

Thanks

Tomoaki yoshida