This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to fast demagnetize solenoid (High frequency solenoid switching)

Other Parts Discussed in Thread: INA250, DRV8801, DRV8840, DRV8840EVM, INA219, INA210, INA215, DRV8829, DRV8842

Hi

I want to switch 24V 2A (to be safe 3A) solenoid with on time of 1ms to 6ms. At present we have kept fixed blank time of 6ms in between two on pulses. But i want to reduce this blanking time. I have gone through "Tips for driving solenoids" And  want to know which will be better solution using DRV8801 or using discrete mosfets  to make my own H-Bridge and then using current sensor like INA250 to detect zero crossing?