Hey,
I have a DRV8850EVM board and am trying to use the external signals (IN1H, IN1L, IN2H, and IN2L) to control a motor. All I could find in the datasheet that I needed to do was to remove resistors R5-R8 and then it should work, but for some reason my output signals are both always held low regardless of what I input. To run the motor forward I have been trying to input PWMs on IN1L and IN1H while I hold IN2L high and IN2H low. I tried switching these signals around, but to no avail. Is there something else that I should be doing to allow the external signals to work? Or is it possible that I am trying to control the signals incorrectly? Any help would be much appreciated.
Thank you!
Charles