1. I want to control brushless DC motor with help Kits DRV8308EVM from extern microcontroller(terminal CLKIN,GND). Is it necessary galvanic isolation microcontroller from terminal CLKIN,GND?
2. Configuration systems: control from computer GUI, DRV8308EVM, brushless DC motor Maxon 118889(no-load speed 11000 ob/min, number of pair poles = 2), open-loop PWM, 120° Commutation, MOD120 = 2048, no load. If PWM Duty Cycle<13% motor don’t spin. Because? What to do to the motor is rotated at PWM Duty Cycle<13%?When PWM Duty Cycle is changed in range 14-20% motor is pulled(example: PWM Duty Cycle=15%, motor rotates with constant speed, set PWM Duty Cycle=18%, motor is pulled and front new constant speed). Because? What to do to the motor is slipped on one speed on other speed? Also same was with motor from Kits DRV8308EVM.