Other Parts Discussed in Thread: DRV10983
I am using DRV10983 demo board and the GUI to control a motor with disk load. Generally the demo board works well, but I want to know whether the DRV10983 can brake the motor with load rotating at high speed if I hope the motor to stop faster. I found that when I turn off the motor (set the motor speed to 0) when the motor is spinning, the motor current goes to 0 immediately, i.e., the controller will not apply power to the motor or absorb power from the motor. I also did not find any setting regarding brake on motor stop.