Hi,
I have 3 different motors, and i Wish to make only one design (not necessary the same components inside) for the 3 motors :
- 15V 20A BLDC (powered from a 4S Li ion battery)
- 30V 25A BLDC (powered by a 7S Li on battery)
- 40V 35A BLDC powered by a 40V custom PSU
Is it possible to have only one design with such different motors ?
(the 15V one is not an obligation but the other 2 i hoe it is possible)
Which booster pack should i take for example ? BOOSTXL-DRV8301 / BOOSTXL-DRV8305 or something else ?
What modifications i have to make to handle 35A ?
I presume the mosfet and Shunt resistor for the current
Thank you
Renaud