Hello,
is there any way to measure the current beeing delivered by the DRV8842 driver to a DC Motor? I have VFREF connected to V3P3OUT with a 47uF filter Capacitor to ground, and use a 0.13ohm sense resistor to allow a maximum current of 5.08A. I know the DRV8801 has a Vprop output, but I need more power, but also need to measure the delivered current. The used microcontroller has an 0-5V ADC, 100Mohm input resistance.
Thank you,
Igor