Hi,
I am looking to use DRV8412 chip to drive a TEC for both heating and cooling operations
Referring to the figure 17 (page 22) in the datasheet, there is two PWM signals that might drive two half bridges, so we should have typically 4 possible cases like below :
PWM A/B = 1 & PWM C/D = 0 => forward, TEC is cooling (for example)
PWM A/B = 0 & PWM C/D = 1 => reverse, TEC is heating (for example)
PWM A/B = 0 & PWM C/D = 0 => slow decay (is it necessary with TEC by the way or fast decay is acceptable ? Even with LC filter as suggested ?)
PWM A/B = 1 & PWM C/D = 1 => useless
Is that true ?