Other Parts Discussed in Thread: DRV8305-Q1
We are using the DRV8305-Q1 part, but having some problems.
First, our part is labeled:
PDRV83055
56TG4
A3DL
Does the 'P' in the part number have significance, i.e., is this some kind of 'pre-release' part?
We're using a SPI interface to write to all of the configuration registers, and I believe this is working correctly. I can read register values, etc.
When we change bit fields for most registers, we see changes on our board, with a scope. However, for the 2 registers x5/x6, HS/LS gate control, when we change the bit fields TDRIVEN/TDRIVEP we don't observe changes on our board. Changing other bit fields in these registers does produce observable changes.
The data sheet we're working from is a 'preliminary' data sheet, date Feb. 2015. We wonder if something has changed, if there is a newer data sheet, and if our part is 'up to date'.
So, are we working with a part that has all the features functional, as described in the data sheet? Should not changing the 2 bit fields TDRIVEN/TDRIVEP produce observable changes?