I have a customer who is currently using a brushed DC motor to drive a fluid pump at 50psi. The pump is closed loop controlled via a pressure sensor. The motor speed is currently adjusted to maintain pressure with the use of a 30kHz PWM of 12VDC. The kicker here may be that it operates with a low side switch, as in the 12VDC line is connected directly to the motor and the ground is switched on and off.
What I am looking for is direction on whether it is feasible to use one of TI's brushless motor control chips as a stand alone device that turns on the motor as soon as power is applied and will vary the speed of the motor using the incoming 30kHz PWM power wires instead of power and a PWM signal wire. This would allow them to run a brushless motor as a drop in replacement without changing the wiring harnesses. The motor currently uses about .4A at 12VDC. I would love it if one of the integrated chips would work like the DRV8313.
Thank you,
Casey