The DRV8825 technical data sheet shows a maximum frequency 250 kHz, The CPG004 GUI instructions tell me that I can set the step frequency but nothing about the allowable maximum. It appears that the software in slvc595/CPG004_RB_MSP430F1612_Firmware_LMD_TI gives me the capability to set it to anything up to 250 kHz.
Logically, there should be issues in realizing a stepping frequency a significant portion of the 35 kHz PWM frequency. I would like to ramp to 5 or 6 kHz. Where will the be a problem?
Presumably, six or seven samples per phase is going to give me some noise. Is there anything else I need to look for?