Using the Evaluation board in the 000 mode.The inductors were removed and the bootstrap capacitors were set to 4.7uF.( c15/18/20/23)
Chanels A & B were driven from two 70 Hz square wave with variable phase between them. Our load was placed between the A and B outputs was a solenoid 15 OHM /0.3H coil.
The system worked causing the solenoid to vibrate as required. However, under some circumstances ( when the input signals had spikes on them????) we caused damage the IC that required it to be changed.
Please tell us the type of conditions that may cause damage to the IC. For example the order of Voltage(12V, 50 V) on was NOT important.