This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8301 sometimes is not running because of GVDD_UV

Other Parts Discussed in Thread: DRV8301

Hello.

There is a problem: if some voltage is present at GVDD pin at rising edge EN_MOTOR then sometimes Charge Pump Regulator is not running and driver report FAULT and GVDD_UV in SPI status register, and GVDD=0V.

If GVDD is about nominal voltage or a little less than nominal then sometimes Charge Pump Regulator is not running at rising edge of EN_MOTOR. If GVDD is at low levels then Charge Pump Regulator is always running.

For now, I make negative pulse of EN_GATE to 300 ms to stable run of DRV8301, after 300 ms GVDD=1.8V. If I make minimum pulse of 11 us then sometimes Charge Pump Regulator is not running and GVDD=0V.


What is minimal treshold of GVDD at rising edge EN_MOTOR to stable running DRV8301? What is nominal of internal resistor to discharge GVDD after falling edge of EN_MOTOR?

Regards,

  Vitaliy Bortsov.

  • Hi Vitaliy,

    We have not heard of this problem before, but will investigate.

    Can you provide your schematic, or a snippet of the schematic with connections on the GVDD pin, output pins, and motor connections?
  • Vitaliy,

    This may be related to the EN_GATE reset pulse. There is a region between the "quick reset" and "full reset" pulses that should not be utilized.

    With the nominal capacitance's from the datasheet a pulse <10us should be applied for a "quick reset" and a pulse >20us should be applied for a "full reset". We have added a note in the rev D datasheet concerning this. Please try this and let me know the results.

  • Hello, Nick.
    Thanks for answer. Indeed, rev.D datasheet is better than rev.A. I read answers for my questions.
    Reset pulses with duration of 20 us doesn't lead to GVDD_UV errors and Charge Pump Regulator run after each pulse normally.

    Regards,
    Vitaliy