This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10983 Issue

Other Parts Discussed in Thread: DRV10983

Hello All,

One of our customer is using DRV10983 for ceiling fan application and able to successfully run the motor with adjusting some parameters.

They have tested the board externally connected to motor and are able to drive it without any initial push to start.

But when they put Board(SMPS+Driver and microcontroller) in Ceiling fan hub, an issue occurred. Motor needs little external push to start. They tried both IPD and Align n Go method. Problem remained same. They are sending speed command by I2C mode.

(Note: Internal Spacing between motor and circuit board is less than 5mm.)

- Does magnetic field of magnets and winding affects DRV or UC?

- Will some adjustments with IPD or Align n GO setting will Solve the problem?

- Does I2C communication fails because of magnetic interference?

- Can we add capacitor w.r.t. ground to each coil to reduce noise?

Awaiting for your valuable help here.