This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Use of DRV 8301-Q1 Without SPI Communication

Other Parts Discussed in Thread: DRV8301-Q1

Hello All,

We are using DRV 8301-Q1 for driving our 2KW board.

We want to test the  board without establishing SPI communication. So are there any default parameter settings in DRV8301-Q1 for parameters which are being set by SPI commands..? Or we must have to use SPI Communication for Making it work..!

Can we use DRV8301-Q1 without SPI communication...?

Awaiting...

Thanks:)