Hi
Can you tell me the differences between DRV2604L and DRV2605L?
regard
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Na:
the major difference is:
DRV2605L has in-chip ROM only, which has Immersion TS2200 inside.
DRV2604L has in-chip RAM only, which can be programmed.
the second difference is:
DRV2605L has audio-to-haptics function, which DRV2604L doesn't.
Hi, Na Na:
Immersion has a software solution TS3000 for Haptics in smartphone. it uses DRV2604L to control the actuator, and also DRV2604L can provide user the best Haptics performance with TS3000.
If customer wants to use DRV2604L to add Haptics effects into his system, it's the customer's own decision whether to contact Immersion.