I am using DRV8811 for my project. I am using DC stepper motor of 1.8 step angle, current 1.5 A rating voltage 4.2 V. I give 3.2 ms pulse to step pin for 120 rpm.
Voltage at Vref is 1.65V. Other component value for RCA,RCB,Isense is exactly same as mentioned in datasheet.My problem is
1) Motor only vibrate internally. Shaft dosen't spin
2) Bout1 & Bout2 dosent work