This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I Can Use the driver DRV8701P?

Other Parts Discussed in Thread: DRV8701

Hello,

I have a Brushed Motor, Model: MY1020 Voltage = 36V,  Rated Current 35,6A  Output = 1000W

I would to like to know if I can use this Driver.

THX.

  • Hi Juan,

    This will depend more on your MOSFET selection for what gate driver is required and heatsinking.

    1000 W is within the DRV8701's capabilities with proper MOSFET selection, heatsinking, and management of the voltage transients. Recommended max voltage for the DRV8701 is 45 V.