I plan to use the DRV8308EVM with a maxon motor that has halls and encoder. A controller will read the encoder position and output CLK and DIR. After connecting the motor and controller to the DRV8308EVM there was a problem even when just commanding pwm mode. The problem is that when running zero speed under a small load, the torque cuts out intermittently and the FAULTn and LOCKn LEDs turn on. This also happens with the DT4269 motor and the DRV8308EVM_GUI in PWM mode. What are the settings that will allow torque control at zero speed?
Thanks,
Stephen