This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8305, control of direction of rotation using one PWM mode, possible?

Other Parts Discussed in Thread: DRV8305

Hello,

I want to use DRV8305 for driving three phase sensored BLDC motor, with PWM_MODE='10' in gate control register 0x7. This is "One single PWM that uses internally stored 6-step block commutation tables", using as input the signals from the three hall sensors.

The question is: Is it possible in this mode to have rotation CCW and rotation CW? I have searched but did not find any bit in any control register that could be used to reverse direction of rotation of the motor.

Regards,

Ivan