Dear Sir
May DRV2700 have webench available?
Best regards,
Bogey
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir
May DRV2700 have webench available?
Best regards,
Bogey
Dear Sir
thanks for you reply~
May we check when we set Gain0=0,Gain1=0,then Gain db(dB) =28.8dB. it is mean AV=27.5??
the input Vp-p is always need 1.8Vp or our intput just under 1.8 Vp. it can normal work.
Best regards,
Bogey
Dear Sir
The customer want to use our EVB to driver 100Vp 2 pcs buzzer(3KHZ 25nF 500Ω)
and use Two Terminal Single Ended Output Configuration (OUT± to BST/GND) and due to customer will use signal generator, so customer will remove MCU.
May we check some item as below:
1.Dose DRV2700 performance is the same between Vdd 3.6V ~ 5v?
2.we will use single ended input ,may i check connect way with you? "C16 connect IN+ and single in. C19 connect GND and IN-" or we can input single from J5??
.we will open JP6/JP5.
3.BST still need connect to PVDD?
Best regards,
Bogey
Hi
Due to the customer will use in test tool, so they will use single generator to DRV2700.
and due to we set to drive 2 buzzer pcs 100 Vp-p, may we check it is mean the load is 2*Cload to heck DS Figure 12. curve.
if one load is 25nf. we chec load is 2*25nf, right? and it is mean when use 50nf, we input frequescy limit around 3K?
and i check DS, DRV2700 should have no OVP function?
Best regards
Bogey
Hello Bogey,
If the total load is 50nF and they are being driven in together in phase, then that should be the load you use. Looking at Fig 12, the bandwidth will not support >3kHz as you mentioned.
Also, the DRV2700 does not have over voltage protection function.
Hope this helps.
Dear
May we also chec if DRV2700 having OCP&OSP function?
Best regards,
Bogey