Other Parts Discussed in Thread: DRV8301
Hello,
We are using a DRV8301 3 phase gate driver in combination with a dsPIC microcontroller.
The only thing I want to to is configuring the current gain amplifier gains at start- up and read these values back to confirm the configuration.
I never get the DRV8301 device to answer.
EN_GATE it set to high and PVDD > 12V
Can you please provide me the correct sequence that I can read registers out of the DRV8301 device.
f CLK = 10MHz
Thanks for a quick reply
Best Regards
Markus