This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Up to 800W sensorless BLDC application

Other Parts Discussed in Thread: DRV8307, DRV8308, DRV8301, DRV8303, DRV8302, DRV8305, UC2625

Motor control applications team,

Here is a question posted under one of our blogs - please help provide your assist to Savas here. Thank you.

hi,

I want to ask a few questions.  I have BLDC sensorless motor. Its specs are 890 rpm/V, 1380 watt peak power, 1080 watt max continuous power, no load current 1.2-1.7 A.  Max continuous current 48 A.  In my project I will use 15.6 Volt battery and I want to reach 700-800 watt power. Can you suggest which control method and driver IC is the best for this solution? thanks in advance for your help

regards

Savas