Hi,
I would like to operate the stepper motor in the indexer mode operation on board not connecting to the GUI of the CPG006_DRV88XX, so can anyone suggest me with the below points how that can be done. The board which I am using is DRV8829 EVM.
* How I can do it in firmware as well as on the board (as per my thinking the indexer mode operation on board is using J10 and J11 connector, please tel me is it correct or no).
* Also please tell me what should be the initial parameters needs to be checked or unchecked in the GUI.