This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV3201-Q1 State change between Global Reset and another state (A-57/58/59)

Other Parts Discussed in Thread: DRV3201-Q1

Hello,

 

Please answer following questions.

 

Q1:

When DRV3201-Q1 is in Active Mode and internal temperature pass over Tmsd2, state changes to Global Reset.

Please advise if DRV3201-Q1 changes to Global Reset when DRV3201-Q1 is in Sleep Mode or Reset State and temperature pass over Tmsd2.

 

Q2:

Please advise minimum VS voltage that DRV3201-Q1 can transition from Global Reset to another state when internal temperature drops below Tmsd0.

Is it 3V or 4.85V?


Q3:

Please conform following state change is correct when temperature drops below Tmsd0 and changes state from Global Reset to another state.

 

Case-1: Change state from Global Reset to Sleep State when EN=Low

Case-2: Change state from Global Reset to Reset State when EN=High and RSTN=Low

Case-2: Change state from Global Reset to Active Mode when EN=High and RSTN=High

 

Best Regards.