This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8308 question

Other Parts Discussed in Thread: DRV8308

Hello,

            Customer have two questions about drv8308

1. Per register 0x00 15:12 bit for Autogain Setpoint, how do we setup this parameters maybe 12 Hz, 3KHZ, 6KHZ....etc? Has any doc or equation to setup it by customer motor spec. and application? 

2. For Clock Frequency Mode, if customer motor spin is 1500 rpm. They enable this mode and CLKIN input 1500 HZ to this pin to get 1500 rpm motor speed, right? if not, how to calculate between motor speed and CLKIN? Thank you. 

BR

Patrick