Other Parts Discussed in Thread: DRV8301, DRV8305
Hello -
I have been doing a lot of learning up on MOSFET characteristics, gate drivers, etc etc. and have pretty much narrowed down to a couple of MOSFETs for my application. The one I am leaning towards is the IRFS3004-7PPbF (http://www.mouser.com/ds/2/200/irfs3004-7ppbf-84182.pdf.
Here are my application specs:
Instaspin-FOC (so 6 MOSFETS switching simultaneously)
20Khz switching frequency
12-35V input range
~100A continuous current (please assume a sound thermal design for the sake of this analysis)
Based on all of the analysis I have done in trying to fit the IRFS3004-7PPbF to the DRV8301, it seems like this should work quite well. But I would love to hear from the pros if there are some aspects I am still missing.
Thanks very much!
-asifjahmed