Hello -
I have a couple of questions regarding reference designs using the DRV8305 (namely the BOOSTXL-DRV8305 and TIDA-00643.
1) Both the BOOSTXL-DRV8305 and the TIDA-00643 reference circuit use a discrete voltage regulator IC for MCU power. Why are they this way, rather than using a DRV83053 with integrated 3.3v LDO? Speaking of the DRV83053, any reference circuits or even just simple diagrams showing the internal LDO in use?
2) On the TIDA-00643, a couple of things. Firstly, the MOSFETs are 30V rated, and so is the overall circuit. How is this possible without any margin between VPDD and VDS? which brings me to question b - the TIDA-00643 uses a TPD4E05U06 TVS protection IC. I get that this provides additional protection to the DRV8305.. but can you please explain the overall reasoning and benefit to using it in this design?
Thanks!
-asifjahmed