This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello everyone,
I am doing a comparative study of the FOC control on BLDC motor and PMSM motor. I have acquired DRV8312-69m kit for that reason (24V, 3.5A..) .The kit features a NEMA 17A BLDC motor with hall sensors. However, now to try out the control algorithms on a PMSM motor, I don't find a PMSM motor of almost similar specifications after searching online through different websites. Can someone help in this regard so as to find a suitable PMSM motor matching the specifications of the DRV8312-69m kit.