This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV104PWPR THERMAL ANALYS

Other Parts Discussed in Thread: DRV104

e2e,

The data sheet for the DRV104 mentions temperature measured on a JEDEC Standard Test Board.  Can you tell me which JEDEC Standard test board was used please?

Thanks for your help.

Regards,

John Wiemeyer 

  • Hi John,

    Our experts have been notified and should reply soon.
  • Hi John,

    I use to provide Applications Engineering support for the DRV104 some years ago, and do have access to some of its archived information. Thus, when I saw this inquiry I wanted to try and provide you with what I know about a likely applicable JEDEC specification, and what I think may be the answer.

    I am fairly certain that the JEDEC specification being referred to in the DRV104 datasheet is JESD51-12, "Guidelines for Reporting and Using Electronic Package Thermal Information." Section 4, "Reporting electronic package thermal results," provides Table 1 — JESD51 Thermal measurement standards by category. Regards PC boards, under the "Boards" title, there is footnote - NOTE 6. That note provides an explanation of two test board cross-sections. The first is a low effective thermal conductivity, referred to as the "1s", or 1 signal plane board. An important point about this board is this board does not have power planes. The "1s" board has a 2 oz/ft finished copper thickness. The second board is a high effective thermal conductivity cross-section referred to as a 2s2p, which has two signal planes and two power planes. 

    If you would like to view JESD52-12, it is available online:

    www.jedec.org/.../jesd51-12.pdf

    Most of the DRV104 development team is no longer with TI, but there are a few people here who had some involvement with it. The two that I did speak with remembered the thermal characterization using a simple board having a single plane. That tends to indicate that the "1s" cross-section board was used. There was even a small even EVM developed for the DRV104.  When I examine one, I find that it uses a single signal layer and has no power planes. It appears to be modeled after the "1s" board. That EVM board uses 1 oz copper, not the 2 oz copper called for in the JEDEC. 

    I hope this helps answer your question.

    Regards, Thomas

    PA - Linear Applications Engineering

  • Hi Thomas,

    I had seen the spec you referred to and concluded that I needed further input from TI to know exactly which of the PB boards TI used for characterization. Thanks for the details you provided which indicate the most likely PC Board TI used was the "1s" board.

    Regards,
    John Wiemeyer
  • Hi John,

    It was my pleasure to assist you.

    Regards, Thomas

    PA - Linear Applications Engineering