This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28069M LAUNCHPAD + BOOST-DRV8848/DRV8711

Other Parts Discussed in Thread: MOTORWARE, DRV8848, BOOST-DRV8848, BOOSTXL-DRV8301, DRV8711

Is there Motorware projects or the equivalent support for using the DRV8848/8711 Booster packs with the F28069M launchpad?

I have the F28069M launchpad currently with the BOOSTXL-DRV8301 and used the Motorware resource to control a BLDC motor. I was hoping to be able to purchase the Boost-DRV8848 and evaluate the device with a BDC motor, looking at the literature it seems that the support is aimed at the MSP430 launchpad.

Could somebody clarify this for me or point me in the direction of relevant information/support please?

Thanks in advance!