We are facing some issues while interfacing DRV8305 with EK-TM4C123GXL board.We have interfaced this with SPI on EK-TM4C123GXL board with single PWM operation mode of DRV8305. but we are not getting the desired output. The BLDC Motor is not rotating.I am attaching the code herewith://***************************************************************************** // // project0.c - Example to demonstrate minimal TivaWare setup // // Copyright (c) 2012-2015 Texas Instruments Incorporated. All rights reserved. // Software License Agreement // // Texas Instruments (TI) is supplying this software for use solely and // exclusively on TI's microcontroller products. The software is owned by // TI and/or its suppliers, and is protected under applicable copyright // laws. You may not combine this software with "viral" open-source // software in order to form a larger program. // // THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS. // NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT // NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR // A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY // CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL // DAMAGES, FOR ANY REASON WHATSOEVER. // // This is part of revision 2.1.1.71 of the EK-TM4C123GXL Firmware Package. // //***************************************************************************** #include <stdint.h> #include <stdbool.h> #include "inc/hw_types.h" #include "inc/hw_memmap.h" #include "driverlib/sysctl.h" #include "driverlib/gpio.h" #include "driverlib/pin_map.h" #include "driverlib/ssi.h" #include "driverlib/uart.h" #include "utils/uartstdio.h" //***************************************************************************** // // Define pin to LED color mapping. // //***************************************************************************** #define RED_LED GPIO_PIN_1 #define BLUE_LED GPIO_PIN_2 #define GREEN_LED GPIO_PIN_3 //***************************************************************************** // // GPIO for PWM Generation for BLDC Motor Driver // //***************************************************************************** #define INHA GPIO_PIN_0 #define INLA GPIO_PIN_1 #define INHB GPIO_PIN_2 #define INLB GPIO_PIN_3 #define INHC GPIO_PIN_4 #define SPI_CS GPIO_PIN_5 //***************************************************************************** // // The error routine that is called if the driver library encounters an error. // //***************************************************************************** #ifdef DEBUG void __error__(char *pcFilename, uint32_t ui32Line) { } #endif //***************************************************************************** // // Main 'C' Language entry point. Toggle an LED using TivaWare. // See www.ti.com/.../project0 for more information and // tutorial videos. // //***************************************************************************** uint8_t ui8_BLDC_State = 0 ; int main(void) { // // Setup the system clock to run at 50 Mhz from PLL with crystal reference // SysCtlClockSet(SYSCTL_SYSDIV_1|SYSCTL_USE_OSC|SYSCTL_XTAL_16MHZ| SYSCTL_OSC_MAIN); // // Enable and configure the GPIO port for the LED operation. // SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF); GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, RED_LED|BLUE_LED|GREEN_LED); // // Enable and configure the GPIO port for the LED operation. // SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB); GPIOPinTypeGPIOOutput(GPIO_PORTB_BASE, INHA|INLA|INHB|INLB|INHC|SPI_CS); // //Enable SSI0 // SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI0); SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA); GPIOPinConfigure(GPIO_PA2_SSI0CLK); GPIOPinConfigure(GPIO_PA3_SSI0FSS); GPIOPinConfigure(GPIO_PA4_SSI0RX); GPIOPinConfigure(GPIO_PA5_SSI0TX); GPIOPinTypeSSI(GPIO_PORTA_BASE, GPIO_PIN_5 | GPIO_PIN_4 | GPIO_PIN_3 | GPIO_PIN_2); SSIConfigSetExpClk(SSI0_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_0, SSI_MODE_MASTER, 100000, 8); // // Enable the SSI0 module. // SSIEnable(SSI0_BASE); // //Send Data on SSI // GPIOPinWrite(GPIO_PORTB_BASE,SPI_CS, SPI_CS); GPIOPinWrite(GPIO_PORTB_BASE,SPI_CS, 0x00); SysCtlDelay(100); SSIDataPut(SSI0_BASE,0x16); SSIDataPut(SSI0_BASE,0x3D); SysCtlDelay(100); GPIOPinWrite(GPIO_PORTB_BASE,SPI_CS, SPI_CS); // // Loop Forever // while(1) { GPIOPinWrite(GPIO_PORTF_BASE,INHA,INHA); SysCtlDelay(10); ui8_BLDC_State++; if(ui8_BLDC_State>12) { ui8_BLDC_State = 1; } switch(ui8_BLDC_State) { case 1: GPIOPinWrite(GPIO_PORTB_BASE,INLA ,0x00 ); GPIOPinWrite(GPIO_PORTB_BASE,INHB ,INHB ); GPIOPinWrite(GPIO_PORTB_BASE,INLB ,INLB ); GPIOPinWrite(GPIO_PORTB_BASE,INHC ,0x00 ); break; case 2: GPIOPinWrite(GPIO_PORTB_BASE,INLA ,0x00 ); GPIOPinWrite(GPIO_PORTB_BASE,INHB ,INHB ); GPIOPinWrite(GPIO_PORTB_BASE,INLB ,0x00 ); GPIOPinWrite(GPIO_PORTB_BASE,INHC ,INHC ); break; case 3: GPIOPinWrite(GPIO_PORTB_BASE,INLA ,0x00 ); GPIOPinWrite(GPIO_PORTB_BASE,INHB ,INHB ); GPIOPinWrite(GPIO_PORTB_BASE,INLB ,0x00 ); GPIOPinWrite(GPIO_PORTB_BASE,INHC ,0x00 ); break; case 4: GPIOPinWrite(GPIO_PORTB_BASE,INLA ,INLA ); GPIOPinWrite(GPIO_PORTB_BASE,INHB ,INHB ); GPIOPinWrite(GPIO_PORTB_BASE,INLB ,0x00 ); GPIOPinWrite(GPIO_PORTB_BASE,INHC ,INHC ); break; case 5: GPIOPinWrite(GPIO_PORTB_BASE,INLA ,INLA ); GPIOPinWrite(GPIO_PORTB_BASE,INHB ,INHB ); GPIOPinWrite(GPIO_PORTB_BASE,INLB ,0x00 ); GPIOPinWrite(GPIO_PORTB_BASE,INHC ,0x00 ); break; case 6: GPIOPinWrite(GPIO_PORTB_BASE,INLA ,INLA ); GPIOPinWrite(GPIO_PORTB_BASE,INHB ,0x00 ); GPIOPinWrite(GPIO_PORTB_BASE,INLB ,0x00 ); GPIOPinWrite(GPIO_PORTB_BASE,INHC ,INHC ); break; case 7: GPIOPinWrite(GPIO_PORTB_BASE,INLA ,INLA ); GPIOPinWrite(GPIO_PORTB_BASE,INHB ,0x00 ); GPIOPinWrite(GPIO_PORTB_BASE,INLB ,0x00 ); GPIOPinWrite(GPIO_PORTB_BASE,INHC ,0x00 ); break; case 8: GPIOPinWrite(GPIO_PORTB_BASE,INLA ,INLA ); GPIOPinWrite(GPIO_PORTB_BASE,INHB ,0x00 ); GPIOPinWrite(GPIO_PORTB_BASE,INLB ,INLB ); GPIOPinWrite(GPIO_PORTB_BASE,INHC ,INHC ); break; case 9: GPIOPinWrite(GPIO_PORTB_BASE,INLA ,INLA ); GPIOPinWrite(GPIO_PORTB_BASE,INHB ,0x00 ); GPIOPinWrite(GPIO_PORTB_BASE,INLB ,INLB ); GPIOPinWrite(GPIO_PORTB_BASE,INHC ,0x00 ); break; case 10: GPIOPinWrite(GPIO_PORTB_BASE,INLA ,0x00 ); GPIOPinWrite(GPIO_PORTB_BASE,INHB ,0x00 ); GPIOPinWrite(GPIO_PORTB_BASE,INLB ,INLB ); GPIOPinWrite(GPIO_PORTB_BASE,INHC ,INHC ); break; case 11: GPIOPinWrite(GPIO_PORTB_BASE,INLA ,0x00 ); GPIOPinWrite(GPIO_PORTB_BASE,INHB ,0x00 ); GPIOPinWrite(GPIO_PORTB_BASE,INLB ,INLB ); GPIOPinWrite(GPIO_PORTB_BASE,INHC ,0x00 ); break; case 12: GPIOPinWrite(GPIO_PORTB_BASE,INLA ,0x00 ); GPIOPinWrite(GPIO_PORTB_BASE,INHB ,INHB ); GPIOPinWrite(GPIO_PORTB_BASE,INLB ,INLB ); GPIOPinWrite(GPIO_PORTB_BASE,INHC ,INHC ); break; } SysCtlDelay(80); GPIOPinWrite(GPIO_PORTF_BASE,INHA,0x00); SysCtlDelay(80); } }