Dear Friends,
I have used DRV8302, as an MOSFET Driver, in my design for BLDC Motor Control Board.
I have a problem, DRV8302 Fault pin always zero. can you give me some advice please??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Rick,
I have run my circuit and Code Composer program. while EnableFlag=1, I have observed the following values.
1) PVDD=25V
2) GVDD=11V
3) AVDD=7V
4) DVDD=3V
5) EN_GATE=3V
6) M_PWM=3.2V
7)
INL_A=3.2V PWM
INL_B=3.2V PWM
INL_C=3.2V PWM
INH_A=3.2V PWM
INH_B=3.2V PWM
INH_C=3.2V PWM
8)
BST_A=11V
BST_B=11V
BST_C=11V
BST_BK=25V PWM
9)
GL_A=0V
GL_B=0V
GL_C=0V
GH_A=1V
GH_B=1V
GH_C=1V