Hello,
Our customer uses the DRV8840, has a question.
There are two pins for Vout. If the one of these pins is opened,
does the OCP trip level change from 6A(min.) to 3A(min.) ?
Regards,
Naoki Aoyama
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Our customer uses the DRV8840, has a question.
There are two pins for Vout. If the one of these pins is opened,
does the OCP trip level change from 6A(min.) to 3A(min.) ?
Regards,
Naoki Aoyama
Hi Naoki,
The outputs are internally connected and there is no such OCP change relationship. Also the outputs should be connected externally.
Best regards,