Hello,
We are doing Induction motor control opertion with following specs:
Input DC voltage: 48V
Motor : 3.5KW operarted at no load
PWM frequency : 20KHz
Observation:
1. Gate driver gets hot when PWM input is given otherwise not
2. Buck converter still works
3. PWM output is not coming
4.Driver(TI DRV8301) has all its default settings.
We are not able to attach the schematic. Please give us a mail id.