This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

survey motor driver request application in IP Cam zoom in/out

Other Parts Discussed in Thread: DRV8812, DRV8811, DRV8846, DRV8880, DRV8885

Hi all,

My customers survey motor driver request application in IP Cam zoom in/out

Driver Request:       
Step motor driver spec       
Logic Supply Voltage:    DC 3.3V
Motor Supply Voltage:    DC12V and DC32V+-15%
Motor current:    500mA   
Microstepping:    Full~1/4   
Operating ambient temperature     –40 85°C   

Please let me know DRV8811 and DRV8812 are suitable this case, if can't, please advise, thanks