This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8824-Q1 9.2.2.2 Current Regulation

Other Parts Discussed in Thread: DRV8824-Q1

Dear sir,

About DRV8824-Q1, Chapter 9.2.2.2  Current Regulation.

Below is our design sample:

For Equation(4):

VREF=3.3V

Rsense=0.4 ohm

=> Ifs = 3.3/(5*0.4) = 1.65 (A)

for Equation(5):

VM=12V

RL=10 ohm(PM25L-024)

Rds=0.63 ohm(room temperature)

Rsense=0.4 ohm

=> Right Equation = 12/(10+2*0.63+0.4)=12/11.66=1.029(A)

So   1.65(A) should small than 1.029(A)?????????????????????????????????

our design is wrong?

Is there any mis-understand of my key parameter input?

But for our real current output, current can reach over 1.3A

No saturated found.

Please help to answer my questions.

Thanks for your support~