Hello Sir/Maam,
please suggest a suitable driver for below mentioned bipolar stepper motor
Model No: BH42 SH 47 - 1704 AF BIPOLAR 4.4 kg cm (0.44 Nm).
Current/Phase:1.7A
Voltage :12-24 V
Application:
Require 8 Stepper motor in one stack to run simultaneously and in synchronization through ATMEGA32 Micro controller
i used only 4 pins to drive 8 stepper motor input pulse from atmega32,is it right way to handle my requirement ?if no please give better solution.