Dear Sir,
If we use CBC mode when OC occurs does it report to Fault pin?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
If we use CBC mode when OC occurs does it report to Fault pin?
During normal operation, CBC is not reported to the FAULT pin. It is expected that the PWM will reset the outputs each cycle.
It is possible during a short to power or ground that the FAULT pin may assert.
Also please note the third paragraph on page 12 of the current datasheet:
It is important to note that if the input to a half bridge is held to a constant value when an over current event occurs in CBC, then the associated half bridge will be in a HI-Z state upon the over current event ending. Cycling IN_X will allow OUT_X to resume normal operation.