Hi,
I really need some input.
We have developed our own BLDC controller cpmpletely based on the schematics for the DRV8301-HC-EVM. Now there is a problem that OCTW asserts low as soon as the DRV8301 is enabled from the F28069M processor. This occurs with or without motor attached. The FETs are ok and all connections are tripple checked. It is correct as far as we can see. This fault actually occurs even with completely detached FETs. What could be the reason for this? We certainly don't have any overcurrents. Is the chip faulty?
Thank you for any ideas!
/Mikael