This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8301-HC-C2-KIT SPI interface wiring

Hello everyone,

My question concerns the user SPI (J8 header). I would like to know which kind of wires I can use to link to these pins ? Can I use a connector ? If yes, which connector I can use ?

Thank you for your time. 

  • Hi Kamal,

    J8 is a 5 pin header with 100 mil pitch. You can use a set of female to male or female to female jumper wires available at most electronic stores.
    Sometimes searching the part number of the J8 header will yield both the J8 connector and the mating connector.