This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using DRV2700 to drive piezoelectric actuator at 500 Hz, 0-150 V

Other Parts Discussed in Thread: DRV2700, DRV2700EVM-HV500, DRV2700EVM

Hello, I am not familiar with electronics but trying to find confidence in purchasing DRV2700.

- Can I uses it to drive piezo actuator at ~ 500 Hz sine wave between 0 to 150V? 

- If I can, what else from 1) Power supply ~5V 2) Analogue sine source 0-3V should I buy?

- For this simple sine wave driving, what PIN configuration should I use?

Best regards,

Jong-Chan