Other Parts Discussed in Thread: DRV8308EVM, DRV8307, DRV8308
Hello,
I am currently looking for a BLDC Controller/Driver/Fet solution with the following specs.
24V DC Sensored BLDC Motor 65W
Must be able to stop & change direction rapidly.
Have internal commutation logic (I can supply PWM & Direction/brake logic signals)
Small footprint. I have room for external mosfets.
If you could recommend a driver IC/Mosfet combination so that I can initiate the design, that would be greatly appreciated.
This is to drive a powered gate.
Kind Regards