This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Material Composition for h-bridge drivers

Hello I have a unique need for an h-bridge driver (basically use it as a controlled DPDT). I need a part that will handle +/- 5A, and in addition it will be used in an MRI environment.. so the material from which it is made matters. Nickel and tin are particularly bad. I would need something constructed and plated with copper, copper alloy, gold, silver (or with similar magnetic susceptibilities).. .. can anyone direct me toward a part? how to find the material compositions?

Cheers

Dean